Paul Desmond

Paul Desmond

  • Connect with me
  • RSS
Paul Desmond is an award-winning writer who has been involved in the IT trade press since 1988. Paul spent 11 years at Network World, serving as a reporter as well as news editor and features editor. Under his leadership, Network World’s features department took home a number of editorial excellence awards, including a 1996 Neal Certificate of Merit Award from the Business Press Association and two 1998 awards from the American Society of Business Press Editors. Paul has also served as editor of Redmond magazine and was the founding editor-in-chief of Redmond Channel Partner magazine, which earned a Neal Award for Best Startup publication of 2005. He has been writing and developing content for MediaSolve Group since 2011.

Catching Up With Long-time Power Expert Clarence Tsung

5.3K views 4 0 1.1K

The Word from VMworld: Prepare for More Virtualization

5.4K views 1 0 706

Modular Data Center Market is Heating up – and Reliability is One Reason

8.6K views 0 0 936

Modular Data Centers Can Help You Stop “Stranding Capital”

4.8K views 0 0 662

Uptime Institute Panel Makes the Case for Modular Data Center Approach

5.7K views 4 0 640

Uptime Institute Event Puts Focus on Modular, Containerized Data Centers

5.3K views 8 0 627

Podcast: An Argument for Open, Suite-based Data Center Management Tools

6.0K views 14 0 827

Podcast: Close-coupled Cooling Delivers Big Energy Savings

30.3K views 27 40 1.7K

AOL Wins Server Roundup Contest, Saves $5 Million by Getting Rid of Old Servers

6.3K views 7 0 786

Podcast: Boost Cooling System Performance with Containment Systems

9.5K views 22 5 974

How IBM Helps Companies Build More Cost-effective, Intelligent Data Centers

4.5K views 3 1 822

Podcast: Economizer Mode Works Wonders for Data Center Cooling – Even in Las Vegas

5.8K views 0 0 895