Stephanie Taylor

Dr. Stephanie Taylor

Dr. Stephanie Taylor is the CEO of Taylor Healthcare Commissioning, Inc. After working as a physician for many decades, Dr. Taylor obtained a Masters in Architecture as well as Infection Control certification. Her lifelong commitment to patient care includes focusing on improving the healthcare physical environment and clinical work processes to help patients heal quickly and save hospitals valuable dollars. Dr. Taylor is a graduate of Harvard Medical School (MD), and Norwich University (Masters Architecture). She has numerous research publications in "Nature", "Science", and other peer-reviewed journals. In her spare time, she enjoys sky-diving, skiing, tennis, SCUBA diving, rock climbing, and road bicycling with her family, as well as playing with her six dogs.

Are Hormones Controlling Hospital Energy Use?

4.9K views 10 1 1.0K

Strategies to maintain hospital thermoregulation and patient comfort

7.7K views 24 0 1.1K

Your Hospital’s Survival Depends on the Ability to Signal and Adjust

17.1K views 43 20 2.4K

Lessons from Biology: Why Your Hospital Needs an Autonomic Nervous System

7.2K views 22 12 1.0K