Services

What’s the best way to maintain an electrical system?

An electrical network is the lifeblood that drives business operations. Network operators and plant managers face a two-fold problem: maintaining their networks to ensure uninterrupted power while dealing with budget cuts, problematic environments, and safety concerns.

Cost-cutting often leads to reduced maintenance team strength and taking an on-demand approach to repairs – which can result in risky maintenance planning.

In fact, the principal reason for electrical system failure is lack of maintenance. All electrical equipment requires regular maintenance to optimize operations, avoid breakdowns, and ensure safety.

998-1237920_GMA-GB_C_

To further complicate matters, the design of many existing electrical infrastructures simply can’t support ever-increasing workload demands. Add to that faulty components and heavy equipment usage, and your maintenance program – or lack thereof – can hinder the performance and life expectancy of your electrical system.

The question is not if a failure will occur, but when. Electrical equipment failure rates are three times higher for components not covered by a scheduled maintenance program, as compared to equipment under a service plan, according to a study published by the Hartford Steam Boiler insurance company.

When developing an effective maintenance program, you’ll want to consider this:

On-demand maintenance

  • Occurs only by request and does not constitute a long-term service provider agreement
  • Doesn’t receive priority response from a service provider
  • Rarely factors in equipment lifecycle issues

Bottom line: Your repair costs may be low, but risk of losses that can impact your business is high.

Service plans

  • Cover standard maintenance and offer “predictive maintenance,” which occurs during system running mode to avoid disruption
  • Estimate and simulate equipment condition over time to assess downtime risks
  • Include parts replacement, system adjustments, and cleaning
  • Offer custom features adaptable to unique business requirements

Bottom line: A structured, planned maintenance program can help you optimize equipment lifespan, control the total cost of ownership, and safeguard human life.

Comparison points of on-demand maintenance vs. service plan approach

Picture2 service plans

If you need to justify transitioning your business from an on-demand practice to a service plan approach, start here:

  • Step 1: Record the number of electrical breakdowns and their impact over the past 5-10 years. Quantify the amount of money spent on correcting electrical faults through on-demand maintenance.
  • Step 2: Contact the electrical equipment manufacturer and request a service plan customized to the nature of the business. The plan should guarantee emergency on-site intervention and delivery of spare parts for immediate corrective action in case of a breakdown.

Investing in a service plan enables you to avoid up to 67% of potential electrical breakdowns and associated financial losses. Service plans reduce overall maintenance expenses and also prolong the lifespan of electrical equipment.

 


2 Responses
  1. Ares

    The number one consideration, of course, is carrying out preventive maintenance as originally scheduled. But this might conflict with the whole grid’s standby reserves and running reserves. In order, therefore, for the grid to have sufficient reserve and for power plant preventive maintenance carried out as scheduled, utilities companies must constantly review – preferably on a quarterly basis – their power development program in coordination with appropriate governing agencies namely: economic, which to me is the number one consideration; environmental, and last but not the least, the type of power plant, i.e. hydro, coal or nuclear, etc., to be put up as programmed in their long or short term development plan; so power plants can be erected on time and in-step with economic growth that would translate to higher electric energy demand. Likewise, all of the proposed plants associated transmission lines and substation including its projected cost should have also been predetermined.

    Reply
    • Denis Koch Denis Koch

      Hi Ares, thanks for your comment, we surely understand the criticalities involved in the maintenance when it comes to power plants and places similar to them.

      However, when the power plant is part of a maintenance program, the on-site operational staff is contacted before-hand. They are informed about the status of their installed electrical system. They can then agree on a date depending upon the type of service contract they have with the provider to perform the needed maintenance. This date is made flexible taking into account all the factors associated with the nature of business. Schneider Electric relies upon its field experience of several years to customize every maintenance program according to client’s business needs, Denis.

      Reply

Leave a Reply to Denis Koch

  • (will not be published)