Services

A Closer Look into the True Cost of Replacing Electrical Switchgear

During my switchgear modernization presentations all over the US, I am constantly reminded of the concerns customers face with their aging electrical infrastructure. For the most part, these center around safety, reliability and productivity:

  • Replacements parts are very hard (or impossible) to be found and priced as an aftermarket product
  • Plants are exposed to forced outages and loss of production due to poor equipment reliability
  • Employee safety is often in question due to slow opening time, increasing the arc flash hazard
  • Arc chutes of old circuit breakers contain asbestos and are not safely maintained
  • Circuit breaker mechanisms have a lot of moving parts, that need lubrication or reconditioning.
  • Low- and medium-voltage switchgear and circuit breakers are beyond their expected useful life.

It gets to a point that engineers of these plants need to decide whether to replace or upgrade existing equipment. Following are 7 factors they should consider in the decision-making process.

    1. The operating environment
    2. The impact of downtime current rating
    3. Cost of ongoing maintenance
    4. Availability of spare parts
    5. The need to increase fault or continuous current rating
    6. Location of existing switchgear
    7. Unforeseen project surprises
modernizaiton electrical switchgear upgrades

I like to compare a switchgear replacement project with a seemingly small house project I recently completed. My wife asked me to replace the old lighting switches in the kitchen of our house, built in 1945. It looked to be an easy and inexpensive project for a Saturday afternoon. I went to the store next to our house and bought the modern switches that she wanted. The project was off to a good start! Back at home, I began work by removing all the cover plates – without using a knife to cut through the paint. As a result, the paint came off with some of the plates, which gave my wife the excuse to repaint all the kitchen walls. To make things a little more dramatic for me, since we were painting the kitchen, she convinced me that it was a good time to replace all the old counter tops to granite! No need to say that my $300 project ended up in the $5000 range.

Similarly, in a switchgear replacement project, plant engineers fund a project based cost $X and can easily end up way over budget because of unforeseen issues. These can include replacing cables, cable trays, pads and doors, or even tearing down walls. All are tasks with an associated cost that were not predicted in the original project scope.

Old low- and medium-voltage switchgear were built like a tank and during normal environment, they should be able to last decades. Circuit breakers can last 25, 30 or even 35 years depending on the maintenance they had during their operations. However, it gets to a point that outdated technology, reliability concerns and maintenance costs cause them to be prohibitive to maintain.

modernization electrical switchgear upgrades

Direct Replacement Solution: Before and after of Westinghouse DB breaker to MasterPact Breaker. Upgrade any brand manufacturer’s brand of switchgear.

Extending the life of low– and medium-voltage switchgear with direct replacement circuit breakers is a very good option that can save over 40% of the total cost of a project. In addition, it allows facility personnel to have more control over the total cost of their project, which can be done in phases over the years.

Read my next post that features a new modernization calculator tool that simulates the total cost of replacing switchgear compared to upgrading switchgear.


2 Responses
  1. Windward Side Electric

    It’s a dreaded project and thought to replace switchgears on large facilities, but like you said with the outages that occur and the loss of production that results, enough electrical outages that link back to aging switchgears will quickly make it obvious that it is time. Looking forward to seeing the calculator you’ve created.

    Reply

Leave a Reply to Windward Side Electric

  • (will not be published)